21.3.51 generate_component

Description

This Tcl command generates a SmartDesign or a core component VHDL code. After generating component, the VHDL file is placed in the <project_folder>/component/work/<component_name> folder.

generate_component -component_name "component_name" \
                   [-recursive 0|1 ]

Arguments

ParameterTypeDescription
component_namestringSpecifies the name of the SmartDesign component or the core component is generated. It is mandatory.
recursiveintegerSpecifies if a SmartDesign component must be generated recursively. It is optional. It is ‘0’ by default and generates only the specified component. If set to ‘1’, all the dependent components, which are in ungenerated state will be generated along with the SmartDesign component. It is recommended to generate all components individually.

Error Codes

Error Code

Description

None

Parameter 'component_name' cannot be empty.

None

recursive: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0 or false).

None

Parameter 'param_name' is not defined. Valid command formatting is 'generate_component [-component_name "component_name"] [-name "name"] [-recursive "TRUE | FALSE"]' .

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command generates SmartDesign "sd2" only.

generate_component -component_name {sd2}

The following command generates SmartDesign "TOP" and all its dependent components, which are in ungenerated state.

generate_component -component_name {TOP} -recursive 1

See Also