21.3.42 export_netlist_file

Description

This Tcl command exports the netlist after the compile state has completed. The netlist can be either Verilog or VHDL. Microchip recommends exporting the netlist after the compile state has successfully completed.

export_netlist_file \
         -file { absolute or relative path and filename for netlist } \
         [-vhdl { value }]

Arguments

ParameterTypeDescription
filestringSpecifies the absolute or relative path and name of netlist file. If specified relative path of netlist file created in <project_name>/designer/<design_name> directory.
vhdlbooleanGenerates the netlist in VHDL (when set to "TRUE" or 1) or Verilog (when set to "FALSE" or 0). Default is 0 (Verilog netlist).

Error Codes

Error CodeDescription
NoneRequired parameter 'file' is missing.

None

vhdl: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0 or false).

None

Parameter 'param_name' is not defined. Valid command formatting is 'export_netlist_file -file "Export Netlist" \ [-vhdl "TRUE | FALSE"] '.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command exports the netlist (Verilog) after the compile state has completed.

export_netlist_files -file {E:/designs/export/sd1/sd1.v} -vhdl 0