User Row Programming Sequence
A Row programming sequence typically includes the following steps, subject to the constraints externally imposed by the Security module:
- Load NVMSRCADR with the address of data in device RAM.
- Load NVMADR with the Flash address to be programmed.
- Configure NVMCON to the Row
program:
- WREN =
1 - PROGOP = 0x2 (see NVMCON)
- WREN =
- Set the WR bit.
- The program sequence completes and the WR bit is cleared by hardware.
- Clear WREN bit to avoid accidental writes.
- Test the WRERR bit to ensure the program sequence completed successfully.
Note: Writes to RAM used during Bus Mastered Row programming cannot be protected.
Consequently, the user must be aware that inadvertent corruption of this area of RAM
is possible during programming.