3.4.3.6.2 PBU Performance Event Outputs
The PBU has event outputs that can be connected to external performance counters at the device level for characterization of the PBU performance. These events can be counted over a period of application execution and compared with the total number of executed instructions and/or the total number of elapsed clock cycles to get a measurement of the PBU efficacy. The performance event signals available from the PBU include:
- Instruction cache “hit” event
- Instruction stream buffer “hit” event
- PBU “hit” event
- Instruction cache “busy” event
The IC hit event indicates when a particular instruction was fetched from the cache memory. The ISB hit event indicates when a particular instruction was fetched from the ISB. This generally happens on the second fetch from a program word while that word is written to the cache memory.
The PBU hit event is of most interest for PBU performance analysis. This event signal is the logical OR of the IC hit and the ISB hit events, and it indicates that the PBU was able to source the requested data without initiating a new NVM fetch.
The IC busy event is used to count the number of extra cycles that were inserted when the ISB could not source the requested data and a Wait state was necessary to determine if the data were available in the IC. An IC busy event is expected to be infrequent and would occur during program flow changes.