3.4.3.6.1 Cache Busy Cycles
The program word is cached on the cycle following the fetch from NVM. During this time, the IC will be busy because of the write-to-cache memory. If the CPU requests program data during this cycle, the PBU will check the contents of the ISB for an address tag match. In most cases, the data may be sourced from the ISB while the IC is busy. This results in an ISB hit and no extra cycle penalty is incurred. When the IC is busy and no ISB hit occurs, then an extra cycle of latency will be inserted while the PBU waits for the IC write cycle to complete. Then, the IC address tags are checked for an IC hit.