2.3.13 PHY_CCAPerform Function
C
PHY_Retval_t PHY_CCAPerform(void)Summary
Perform a clear channel assessment
Description
This function is used to perform a clear channel assessment on current channel. using configured CCA mode (can be set using PHY_PibSet of phyCCAMode). This results in the status of channel is current busy or Idle.
The different CCA modes supported by Transceiver are The CCA mode
CCA Mode 1: Energy above threshold. CCA shall report a busy medium upon detecting any energy above the ED threshold.
CCA Mode 2: Carrier sense only. CCA shall report a busy medium only upon the detection of a signal with the modulation and spreading characteristics of IEEE 802.15.4. This signal may be above or below the ED threshold.
CCA Mode 3: Carrier sense with energy above threshold. CCA shall report a busy medium only upon the detection of a signal with the modulation and spreading characteristics of IEEE 802.15.4 with energy above the ED threshold.
Precondition
PHY_Init() should have been called before calling this function.
Parameters
None
Returns
PHY_CHANNEL_IDLE - The CCA attempt has detected an idle channel
PHY_CHANNEL_BUSY - The CCA attempt has detected a busy channel
Example
PHY_Retval_t retVal = PHY_FAILURE; uint8_t phyChannel = 15; PibValue_t pibValue; bool isChIdle = false; // Setting Current channel pibValue.pib_value_8bit = phyChannel; retVal = PHY_PibSet(phyCurrentChannel, &pibValue); if(PHY_SUCCESS == retVal) { //Take the Ed sample retVal = PHY_CCAPerform(); if (PHY_CHANNEL_IDLE == retVal) { isChIdle = true; } }
Remarks
None