2.3.9 PHY_RxFrameCallback Function
C
void PHY_RxFrameCallback(PHY_FrameInfo_t *rxFrame)Summary
User callback function for the reception of a frame
Description
This callback function SHOULD be defined by the upper layer(Application/MAC) for getting the received frame details
Precondition
This is a Asynchronous function call for the reception of a frame
Parameters
| Param | Description |
|---|---|
| rxFrame | Pointer to received frame structure of type PHY_FrameInfo_t or to received frame array |
| rxFrame->buffer_header - BMM Buffer Header of the frame | |
| rxFrame->mpdu - Actual MPDU comprises of | |
| mpdu - Payload Length(N) | |
| mpdu- Payload mpdu- LQI of received packet | |
| mpdu- ED_LEVEL of received packet |
Returns
None
Example
uint8_t rxBuffer[LARGE_BUFFER_SIZE]; uint8_t frameLen, frameLQI, frameED; int8_t frameRSSI; void PHY_RxFrameCallback(PHY_FrameInfo_t *frame) { printf("\n--RxCallbackreceived--"); frameLen = frame->mpdu[0]; //Copy the payload memcpy(rxBuffer, (uint8_t *)&(frame->mpdu[1]), frameLen); //Copy the LQI frameLQI = frame->mpdu[frameLen+LQI_LEN]; //Copy the RSSI frameED = frame->mpdu[frameLen+LQI_LEN+ED_VAL_LEN]; frameRSSI = (int8_t)(frameED + PHY_GetRSSIBaseVal()); // free the buffer that was used for frame reception bmm_buffer_free((buffer_t *)(frame->buffer_header)); }
Remarks
bmm_buffer_free SHOULD be called in the PHY_RxFrameCallback() for reusing the buffer for reception. Otherwise no buffers will be availble for reception. Number of buffers can be increased by changing the NUMBER_OF_LARGE_PHY_BUFS in stack_config.h. By default, the value is 3. If the buffer is not freed upon receiving the packet, transceiver can receive upto NUMBER_OF_LARGE_PHY_BUFS (3) frames only.