2.3.28 PHY_GetTrxConfig Function
C
PHY_Retval_t PHY_GetTrxConfig(PHY_ConfigParam_t parameter, uint8_t *paramValue)Summary
To read a current setting of particular transceiver parameter
Description
The function is used to read the current of particular parameter. The following parameters can be read from TRX, | Param | Description | |:----- |:----------- | |ANT_DIVERSITY|Antenna Diversity| |ANT_SELECT|Antenna Configured - ANTENNA_1/ANTENNA_2| |ANT_CTRL|Antenna Control| |AACK_PROMSCS_MODE|Promiscuous Mode| |TX_PWR|Tx Power Configured| |RX_SENS|Rx Sensitivity| |RX_RPC|RX Reduced Power Consumption| |RX_AUTO_ACK|Automatic acknowledgement| |RX_RESERVED_FRAME|Reserved frame reception| |FILTER_RESERVED_FRAME|Filter reserved frame|
Precondition
PHY_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| parameter | Type of the parameter to be read |
| paramValue | Pointer to the current parameter value |
Returns
PHY_INVALID_PARAMETER - If the parameter is invalid
PHY_SUCCESS - otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
bool promCtrl = true;
// To get the promiscuous mode configured
PHY_GetTrxConfig(AACK_PROMSCS_MODE, (uint8_t *)&promCtrl);Remarks
None