2.3.19 PHY_ConfigReservedFrameFiltering Function
C
PHY_Retval_t PHY_ConfigReservedFrameFiltering(bool recReservedFrame,
bool bypassFrameFilter )Summary
Configures TRX for receiving reserved frame
Description
This function is used to configure the trx for receiving the reserved frame type frames and to enable/disable the frame filtering .
Precondition
PHY_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| recReservedFrame | true to enable the reception of reserved frame types acknowledgment after reception |
| bypassFrameFilter | true to bypass the frame filtering at the hardware level like data frame as specified in IEEE specification |
Returns
PHY_SUCCESS If trx is configured correctly PHY_FAILURE otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
bool rxResFrame = true;
bool bypassFrameFiltering = false;
retVal = PHY_ConfigReservedFrameFiltering(rxResFrame, bypassFrameFiltering);
if(PHY_SUCCESS == retVal)
{
//Trx is configured to receive the reserved frame and to do the frame
//filtering as stated in IEEE Spec
}Remarks
None