2.3.29 PHY_GetSWVersion Function
C
uint32_t PHY_GetSWVersion(void)Summary
To Get the current Software version of PHY
Description
This function is used Get the current Software version of PHY
Precondition
PHY_Init() should have been called before calling this function
Parameters
None
Returns
32-bit PHY SW version value
Example
uint32_t phySwVersion; // Get sw version of the PHY phySwVersion = PHY_GetSWVersion();
Remarks
None