2.3.12 PHY_EdSample Function
C
uint8_t PHY_EdSample(void)Summary
Perform a single ED measurement on current channel
Description
This function is used to measure the energy level on current channel
Precondition
PHY_Init() should have been called before calling this function.
Parameters
None
Returns
edValue - Result of the measurement
Example
PHY_Retval_t retVal = PHY_FAILURE; uint8_t phyChannel = 15; uint8_t edLevel; int8_t pwrDbm; PibValue_t pibValue; // Setting Current channel pibValue.pib_value_8bit = phyChannel; retVal = PHY_PibSet(phyCurrentChannel, &pibValue); if(PHY_SUCCESS == retVal) { //Take the Ed sample edLevel = PHY_EdSample(); //Convert the energy level to input power in Dbm pwrDbm = (int8_t)(edLevel + PHY_GetRSSIBaseVal()); }
Remarks
PHY_EdSample scans the channel for 8 symbols(128us) and returns the energy level