2.3.4 PHY_PibSet Function
C
PHY_Retval_t PHY_PibSet(uint8_t attribute, PibValue_t *value)Summary
Sets the PHY PIB attribute with value
Description
This function is called to set the transceiver information base attributes. The list of PHY PIB attributes, its default values and range are described in the above table. For more information refer ieee_phy_const.h file
Precondition
PHY_init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| attribute | PHY infobase attribute ID |
| value | Pointer to the PHY infobase attribute value to be set |
Returns
PHY_UNSUPPORTED_ATTRIBUTE - if the PHY info base attribute is not found
PHY_BUSY - If the PHY is not in PHY_IDLE state.An exception is macBeaconTxTime which can be accepted by PHY even if PHY is not in PHY_IDLE state
PHY_SUCCESS - If the attempt to set the PIB attribute was successful
PHY_TRX_ASLEEP - If trx is in SLEEP mode and access to trx is required
Example
PHY_Retval_t retVal = PHY_FAILURE; uint8_t phyChannel = 15; uint8_t shortAddr = 0x1234; PibValue_t pibValue; // Setting Current channel pibValue.pib_value_8bit = phyChannel; retVal = PHY_PibSet(phyCurrentChannel, &pibValue); if(PHY_SUCCESS == retVal) { //Channel is configured } //Setting short Address pibValue.pib_value_16bit = shortAddr; retVal = PHY_PibSet(macShortAddr, &pibValue); if(PHY_SUCCESS == retVal) { //Short Address is configured }
Remarks
None