2.3.11 PHY_EdEndCallback Function
C
void PHY_EdEndCallback(uint8_t energyLevel)Summary
User callback function for Energy detection
Description
This function SHOULD be defined by the upperlayer (Application/MAC layer) in order to get the energyLevel on the current channel which is being scanned for a period of scanDuration symbols
Precondition
This is an Asynchronous function call for the energy scan complete
Parameters
| Param | Description |
|---|---|
| energyLevel | Measured energy level during ED Scan With energy_level, the RF input power can be calculated as follows |
| PRF = RSSI_BASE_VAL + 1 x energy_level |
Returns
None
Example
void PHY_EdEndCallback(uint8_t energyLevel)
{
int8_t energyLeveldBm = (int8_t) (PHY_GetRSSIBaseVal() + energyLevel);
energyLevel = energyLevel;
}Remarks
None