2.3.10 PHY_EdStart Function
C
PHY_Retval_t PHY_EdStart(uint8_t scanDuration)Summary
Starts Energy Detection Scan
Description
This function starts an ED Scan for the scan duration specified by the upper layer. Actual ED result of Energy level on current channel will be indicated by PHY_EdEndCallback(eneryLevel). Scan duration formula:
aBaseSuperframeDuration x (2^SD + 1) symbols
where SD - scanDuration parameter (0 - 14)
Precondition
PHY_Init() should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| scanDuration | Specifies the ED scan duration in symbols |
| Range - (0 to 14) |
Returns
PHY_SUCCESS - ED scan is started successfully
PHY_BUSY - PHY is busy servicing the previous request
PHY_TRX_ASLEEP - Transceiver is currently sleeping, wakeup the transceiver using PHY_TrxWakeup() function
PHY_FAILURE - otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
uint8_t scanDurationSym = 1;
retVal = PHY_EdStart(scanDurationSym);
if (PHY_SUCCESS =! retVal)
{
//ED scan cannot be started at this moment
}Remarks
PHY_EdEndCallback(energyLevel) will be called after scanning the current channel for a time period of aBaseSuperframeDuration x (2scanDuration + 1) symbols. For scanDuration of value 0, ScanTime = 960 x(20 +1) = 1920 symbols = 30720 us.