2.3.3 PHY_Reset Function
C
PHY_Retval_t PHY_Reset( bool setDefaultPibs )Summary
Resets the PHY Layer
Description
This function is called to Resets PHY state machine and sets the default PIB values if requested
Precondition
PHY_Init() should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| setDefaultPibs | Defines whether PIB values need to be set to its default values |
Returns
PHY_SUCCESS - If the transceiver state is changed to TRX_OFF and PIBs are set to their default value
PHY_FAILURE - Otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
bool setDefault = false;
retVal = PHY_Reset(setDefault);
if (PHY_SUCCESS =! retVal)
{
while(1);
}Remarks
None