2.3.5 PHY_PibGet Function
C
PHY_Retval_t PHY_PibGet(uint8_t attribute, uint8_t *value)Summary
Gets a PHY PIB attribute
Description
This function is called to retrieve the transceiver information base attributes. The list of PHY PIB attributes, its default values and range are described in the above table. For more information refer ieee_phy_const.h file
Precondition
PHY_init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| attribute | PHY infobase attribute ID |
| value | Pointer to the PHY infobase attribute value |
Returns
PHY_UNSUPPORTED_ATTRIBUTE - If the PHY infobase attribute is not found
PHY_SUCCESS - otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
uint8_t phyChannel;
uint8_t shortAddr;
// Getting Current channel
retVal = PHY_PibGet(phyCurrentChannel, &phyChannel);
if(PHY_SUCCESS == retVal)
{
printf("\r\n PHY Current Channel - %d",phyChannel );
}
//Getting short Address
retVal = PHY_PibGet(macShortAddr, &shortAddr);
if(PHY_SUCCESS == retVal)
{
printf("\r\n Device short addr - 0x%x",shortAddr );
}
Remarks
None