2.3.23 PHY_ConfigTxPwr Function
C
PHY_Retval_t PHY_ConfigTxPwr(bool type, int8_t pwrValue)Summary
Configures the TX Power in Transceiver
Description
This function is used to configure the Transmit power of the transceiver
Precondition
PHY_Init() should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| type | PWR_REGISTER_VALUE or PWR_DBM_VALUE |
| pwrValue | Index of the power register value (0-15) or Power value in dBm (-14dBm to 12dBm) |
Returns
PHY_SUCCESS - If pwrValue bit is configured correctly
PHY_FAILURE - Otherwise
Example
bool pwrType = PWR_REGISTER_VALUE; uint8_t pwrIndex = 0x00; bool configStatus = false; //Set Tx Power with Register Index value if (PHY_SUCCESS == PHY_ConfigTxPwr(pwrType, int8_t (pwrIndex))) { configStatus = true; } //Set Tx Power with dBm value int8_t pwrDbm = -12; pwrType = PWR_DBM_VALUE; if (PHY_SUCCESS == PHY_ConfigTxPwr(pwrType, int8_t (pwrDbm))) { configStatus = true; } uint8_t pwrReg; // To get the tx power index value configured in the TRX PHY_GetTrxConfig(TX_PWR, &pwrReg);
Remarks
None .