2.3.15 PHY_StopContinuousTransmit Function
C
void PHY_StopContinuousTransmit(void)Summary
Stops the continuous transmission on the current channel
Description
This function is called to stop the continuous transmission
Precondition
PHY_Init() should have been called before calling this function. This function will stop the continuous transmission which is started by PHY_StartContinuousTransmit()function.
Parameters
None
Returns
None
Example
PHY_Retval_t retVal = PHY_FAILURE; uint8_t phyChannel = 15; PHY_ContinuousTxMode_t txMode = PRBS_MODE; bool useRandomContent = true; bool contTxStarted = false; PibValue_t pibValue; // Setting Current channel pibValue.pib_value_8bit = phyChannel; retVal = PHY_PibSet(phyCurrentChannel, &pibValue); if(PHY_SUCCESS == retVal) { //Start continuous tx in CW mode PHY_StartContinuousTransmit(txMode, useRandomContent); contTxStarted = true; } if(contTxStarted) { //Stop continuous tx PHY_StopContinuousTransmit(); }
Remarks
When continuous tx is stopped, the PHY_Reset function is called. User has to reconfigure the configuration parameters (PHY_ConfigParam_t) which are set by application.