2.3.25 PHY_ConfigAntennaDiversity Function
C
PHY_Retval_t PHY_ConfigAntennaDiversity(bool divCtrl, uint8_t antCtrl)Summary
Configures antenna diversity and selects antenna
Description
This function is used to enable the Antenna Diversity feature and to select the antenna path if the feature is disabled. Antenna Diversity uses two antennas to select the most reliable RF signal path. To ensure highly independent receive signals on both antennas, the antennas should be carefully separated from each other. If a valid IEEE 802.15.4 frame is detected on one antenna, this antenna is selected for reception. Otherwise the search is continued on the other antenna and vice versa.
Precondition
PHY_Init() should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| divCtrl | true/false to enable/disable antenna diversity algorithm |
| antCtrl | 0 or 3 when antenna diversity is enabled 1 or 2 to select antenna 1 or antenna 2 |
Returns
PHY_SUCCESS - If Antenna Diversity/ Control bits are configured correctly
PHY_FAILURE - otherwise
Example
bool antDiv = ANTENNA_DIVERSITY_DISABLE; uint8_t antennaSel = ANTENNA_CTRL_1; // Antenna Diversity is disabled and Antenna 1 is selected for rx/tx path PHY_ConfigAntennaDiversity(antDiv, antennaSel); // To get the antenna diversity value configured in the TRX PHY_GetTrxConfig(ANT_DIV, &antDiv); // To get antenna selected for rx/tx PHY_GetTrxConfig(ANT_SELECT, &antennaSel);
Remarks
None