2.3.18 PHY_ConfigAutoAck Function
C
PHY_Retval_t PHY_ConfigAutoAck(bool enableAACK)Summary
Configures TRX for auto acknowledging the reserved frame
Description
The function is used to configure the automatic acknowledgment from Transceiver after packet reception. By default, Automatic Acknowledgement after reception is enabled.
Precondition
PHY_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| enableAACK | true - To Disable automatic acknowledgment after reception |
| false - to enable the automatic acknowledgment after reception |
Returns
- PHY_SUCCESS - If trx is configured correctly
- PHY_FAILURE - otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
bool isDisableAACK = false;
retVal = PHY_ConfigAutoAck(isDisableAACK);
if(PHY_SUCCESS == retVal)
{
//Trx is configured to auto acknowledge for the received packet
}Remarks
None