2.3.17 PHY_TrxWakeup Function
C
PHY_Retval_t PHY_TrxWakeup(void)Summary
Wakes up the transceiver from sleep
Description
This function awakes the transceiver from sleep state.
Precondition
PHY_TrxSleep() should have been called before calling this function
Parameters
None
Returns
PHY_TRX_AWAKE - The transceiver is already awake
PHY_SUCCESS - The transceiver is woken up from sleep
PHY_FAILURE - The transceiver did not wake-up from sleep
Example
PHY_SleepMode_t sleepMode = SLEEP_MODE_1;
bool trxSleepStatus = false;
// Set Transceiver to sleep
if (PHY_SUCCESS == PHY_TrxSleep(sleepMode))
{
trxSleepStatus = true;
}
//wakeup the transceiver
if (PHY_SUCCESS == PHY_TrxWakeup())
{
trxSleepStatus = false;
}Remarks
When TRX is put into DeepSleep, the TRX registers are reset and it will hold default values, PIB values are getting written by PHY layer when Wakeup function is called.User has to reconfigure the configuration parameters (PHY_ConfigParam_t) which are set by application. This procedure is not needed for SLEEP mode as the TRX register values are retained.