2.3.20 PHY_ConfigRxPromiscuousMode Function
C
PHY_Retval_t PHY_ConfigRxPromiscuousMode(bool promCtrl)Summary
Configures RX promiscuous mode
Description
This function is used to enable the RX promiscuous mode. The TRX will receive all frames even with FCS failure, PHY layer will discard the CRC invalid packet and TRX will not acknowledge even ack is requested by the received packet(auto ack is disabled in this mode).
Precondition
PHY_Init() should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| promCtrl | true to enable promiscuous mode |
| false to disable promiscuous mode |
Returns
PHY_SUCCESS - If promCtrl bits are configured correctly
PHY_FAILURE - otherwise
Example
bool promCtrl = true; // Enable Promiscuous mode PHY_ConfigRxPromiscuousMode(promCtrl); // To get the PDT level configured PHY_GetTrxConfig(AACK_PROMSCS_MODE, &promCtrl);
Remarks
None