2.3.26 PHY_GetTrxStatus Function
C
PHY_TrxStatus_t PHY_GetTrxStatus(void)Summary
Returns the current status of the Transceiver
Description
This function gets the status of the transceiver
Precondition
PHY_Init() should have been called before calling this function
Parameters
None
Returns
PHY_TRX_OFF - The transceiver is in TRX_OFF state
PHY_RX_ON - The transceiver is in receive state
PHY_TX_ON - The transceiver is in Transmit state
PHY_BUSY_RX - The transceiver currently receiving the packet
PHY_BUSY_TX - The transceiver is currently transmitting the packet
PHY_TRX_SLEEP - The transceiver is in sleep state
PHY_DEEP_SLEEP - The transceiver is in Deep sleep state
Example
PHY_TrxStatus_t trxStatus; //Gets the current status of trx trxStatus = PHY_GetTrxStatus();
Remarks
None .