2.3.30 PHY_IsFramePendingFromNextLayer Function
C
bool PHY_IsFramePendingFromNextLayer(PHY_Addr_t *addr, uint8_t *addrMode)Summary
Function to check whether Any frame is pending from higher layer upon reception of Datarequest command frame (Ex: MAC/APP).
Description
Function to check whether Any frame is pending from higher layer upon reception of Datarequest command frame (Ex: MAC/APP) so that the automatic acknowledgement frame will have proper FramePending bit status
Precondition
PHY_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| addr | Source Address of the Datarequest (Either Short/Long) frame received |
| addrMode | Either FCF_SHORT_ADDR or FCF_LONG_ADDR |
Returns
true - If Frame is pending for the RFD false - Otherwise
Example
bool PHY_IsFramePendingFromNextLayer(PHY_Addr_t *addr, uint8_t *addrMode)
{
bool isFramePending = true;
return isFramePending;
} Remarks
This function is invloked by phy layer on the reception of Datarequest frame in ISR context. The higher layer has to implement this function approprietely to set the framepending bit in Acknoewledgement frame. This function is weak by default with FramePending bit set to true.