2.3.2 PHY_Init Function
C
PHY_Retval_t PHY_Init( void )Summary
Initialization of PHY Layer
Description
This function is called to initialize the PHY layer. The transceiver is initialized and it will be in PHY_STATE_TRX_OFF, the PHY PIBs are set to their default values. PAL layer is initialized
Precondition
SYS_Load_Cal(WSS_ENABLE_ZB) function of device support library should be called before calling this function.
Parameters
None.
Returns
PHY_SUCCESS - If the transceiver state is changed to TRX_OFF
PHY_FAILURE - Otherwise
Example
PHY_Retval_t retVal = PHY_FAILURE;
retVal = PHY_Init();
if (PHY_SUCCESS =! retVal)
{
while(1);
}Remarks
This routine must be called before any of the PHY function is called