3.3.23.6 tmcRef_State_s Struct
C
// Floating point structure defining the state of the reference control module.
typedef struct
{
bool enable; /* Flag indicating reference control module enable status */
bool initDone; /* Flag indicating reference control module initialization status */
float32_t lowerLimit; /* Lower limit for the reference value */
float32_t upperLimit; /* Upper limit for the reference value */
float32_t reference; /* The current reference value that the speed control uses */
float32_t rampRate; /* The rate at which the reference value is allowed to change per control cycle */
}tmcRef_State_s;
// Fixed point structure defining the state of the reference control module.
typedef struct
{
bool enable; /* Flag indicating reference control module enable status */
bool initDone; /* Flag indicating reference control module initialization status */
int16_t_t lowerLimit; /* Lower limit for the reference value */
int16_t_t upperLimit; /* Upper limit for the reference value */
int32_t scaledLowerLimit; /* Scaled lower limit for the reference value */
int32_t scaledUpperLimit; /* Scaled upper limit for the reference value */
int32_t scaledReference; /* Scaled reference value */
int32_t scaledRampRate; /* Scaled ramp rate */
int16_t reference; /* Reference value */
} tmcRef_State_s;
Summary
Reference control Module Structure.
Description
This structure holds the parameters for the reference control module. It includes control flags, speed reference value, its limits, and the rate of change (ramp rate).
Remarks
Refer the generated header file for the exact typedef signature..