1.1.5.66 SPW_PKTTX_SetNextSendList
void SPW_PKTTX_SetNextSendList(uint8_t* routerBytesTable,
SPW_PKTTX_SEND_LIST_ENTRY* sendListAddress,
uint16_t length,
bool abort,
SPW_PKTTX_NXTSEND_START startMode,
uint8_t startValue)
Summary
Set the SPW next send list informations and start conditions
Preconditions
None
Parameters
routerBytesTable - Table of 4 router bytes to prepend (if non-zero) to each packets in the send list. All bytes are set to 0 if this pointer is NULL
sendListAddress - Pointer to the send list type object that will be transmitted
length - Number of entries in send list
abort - Set to True if any ongoing send list should be abort when this send list wants to start
startMode - Send list start mode condition
startValue - Matching value for event start condition
Returns
None