12.2.2 Port List
The following table lists MMUART I/O signals. X is used as a place holder for 0 or 1 in register and signal descriptions, indicating MMUART_0 or MMUART_1.
| Name | Type | Polarity | Description |
|---|---|---|---|
| MMUART_X_CTS | Input | Low | Clear to send. This signal is used in the modem interface. The active-low signal is an input that indicates when the attached device (modem) is ready to accept data. MMUART passes the information to the Cortex-M3 processor through the modem status register (Table 12-20). The register indicates that the CTSn signal is changed since the register is read last time. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_DSR | Input | Low | Data set ready. This signal is used in modem interface. The active-low signal is an input that indicates when the attached device (modem) is ready to set up a link with MMUART. MMUART passes the information to the Cortex-M3 processor through the Table 12-20. This register also indicates that the DSRn signal is changed since the register was read last time. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_DCD | Input | Low | Data carrier detect. This signal is used in the modem interface. The active-low signal is an input that indicates when the attached device (modem) has detected a carrier. MMUART passes this information to the Cortex-M3 processor through the Table 12-20. This register also indicates that the DCDn signal is changed since the register is read last time. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_RI | Input | Low | Ring indicator. This signal is used in the modem interface. The active-low signal is an input showing when the attached device (modem) senses a ring signal on the telephone line. MMUART passes this information to the Cortex-M3 processor through the Table 12-20. This register also gives an indication when the RI trailing edge is sensed. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_RTS | Output | Low | Request to send. This signal is used in the modem interface. The active-low output signal is used to inform the attached device (modem) that MMUART is ready to send data. It is programmed by the Cortex-M3 processor through the Table 12-18. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_DTR | Output | Low | Data terminal ready. This signal is used in the modem interface. The active-low output signal informs the attached device (modem) that MMUART is ready to establish a communications link. It is programmed by the Cortex-M3 processor through the Table 12-18. This signal can either go to the fabric or to the I/O pad. |
| MMUART_X_RXD | Input | Serial input data This is the data transmitted into MMUART. It is synchronized with the APB clock (master clock) input pin. This signal can either go to the fabric or to the I/O pad. | |
| MMUART_X_TXD | Output | Serial output data. This is the data transmitted from MMUART. It is synchronized with the BAUDOUT output pin. This signal can either go to the fabric or to the I/O pad. | |
| MMUART_X_SCK_IN | Input | Serial input synchronous clock. The MMUART_X_SCK can be configured as an input synchronous clock from master when the MMUART_X acts as a slave. | |
| MMUART_X_SCK_OUT / BAUDOUTN | Output | Low | In Synchronous mode, it is the serial output
clock, SCK_OUT. MMUART_X_SCK can be configured as an output synchronous clock
to a slave when MMUART_X acts as a master. In Asynchronous mode, it is the baud rate clock derived from APB_X_CLK and BAUDOUTN. |
| MMUART_X_ESWM | Output | High | Single-wire, half-duplex enable. If this signal is active-high, then the data I/O is configured for half-duplex operation over a single-wire, using the Tx pad (out signal). If Low, then the data I/O has separate Tx (out) and Rx (in) pins. Single-wire mode enable (ESWM) signal goes to the FPGA fabric, when it can be used on any pad. |
| MMUART_X_TE | Output | High | Transmitter output enable. This active-high signal is used as a bi-directional enable for single-wire half-duplex operation. An active-high signal transmits out, and a Low signal is received. TE usage implies that the MMUART is configured in single-wire mode with the single-wire mode (SWM) bit. |
| MMUART_X_E_MST_SCK | Output | High | Enable master clock. This active-high signal is used as a bi-directional enable for the SCK_IN and SCK_OUT signals. If these signals are taken from a single bi-directional pad, E_MST_SCK active-high designates Master mode and forces the bi-directional pad as an output. Otherwise (in case of active-low), the pad is an input for SCK_IN. |
| MMUART_X_OUT1 | Output | Low | Output 1. This active-low output is a user-defined signal. It is programmed by the processor via the Table 12-18 and is set to the opposite value. It can be used as a bi-directional pad enable for bi-directional topology use models. |
| MMUART_X_OUT2 | Output | Low | Output 2. This active-low output signal is a user-defined signal. It is programmed by the processor via the Table 12-18 and is set to the opposite value. |