22.3.2.2.1 Software Design Flow

The software design flow consists of enabling the MSS to the fabric interrupts.

Enabling the MSS to the Fabric interrupt

The interrupt enable registers do not affect the Cortex-M3 process or the NVIC; these are per bit enables of the interrupt routed to the FPGA fabric. It enables the MSS to fabric interrupt, MSS_INT_M2F, by setting the following INTERRUPT_ENABLE0 or INTERRUPT_ENABLE1 register bit-band.

INTERRUPT_CTRL_BITBAND-> bit-band register bit of INTERRUPT_ENABLE0 or INTERRUPT_ENABLE1 = <1/0>;

The following table gives the bit-band register bit of INTERRUPT_ENABLE0 and INTERRUPT_ENABLE1 in INTERRUPT_CTRL structure. See m2sxxx.h contained in the CMSIS folder.

Table 22-4. Bit-Band Register Bit of Interrupt_Enable0 and Interrupt_Enable1
Bit-Band Register Bit
INTERRUPT_ENABLE0INTERRUPT_ENABLE1
SPIINT0_ENBLRESERVED1[3]
SPIINT1_ENBLMDDR_IO_CALIB_INT_ENBL
I2C_INT0_ENBLRESERVED2
I2C_INT1_ENBLFAB_PLL_LOCK_INT_ENBL
MMUART0_INTR_ENBLFAB_PLL_LOCKLOST_INT_ENBL
MMUART1_INTR_ENBLFIC64_INT_ENBL
MAC_INT_ENBLRESERVED3[24]
USB_MC_INT_ENBL—
PDMAINTERRUPT_ENBL—
HPD_XFR_CMP_INT_ENBL—
TIMER1_INTR_ENBL—
TIMER2_INTR_ENBL—
CAN_INTR_ENBL—
RTC_WAKEUP_INTR_ENBL—
WDOGWAKEUPINT_ENBL—
MSSDDR_PLL_LOCKLOST_INT_ENBL—
ENVM_INT0_ENBL—
ENVM_INT1_ENBL—
I2C_SMBALERT0_ENBL—
I2C_SMBSUS0_ENBL—
I2C_SMBALERT1_ENBL—
I2C_SMBSUS1_ENBL—
HPD_XFR_ERR_INT_ENBL—
MSSDDR_PLL_LOCK_INT_ENBL—
SW_ERRORINTERRUPT_ENBL—
DDRB_INTR_ENBL—
ECCINTR_ENBL—
CACHE_ERRINTR_ENBL—
SOFTINTERRUPT_ENBL—
COMBLK_INTR_ENBL—
USB_DMA_INT_ENBL—
RESERVED0—

To enable the MSS to the fabric interrupts, listed in the Select Group 0 or Select Group 1 column of Table 22-1, set the bit-band register bit of INTERRUPT_MODE register as follows:

INTERRUPT_CTRL_BITBAND-> SELECT_MODE= <1/0>;

Monitoring the MSS to the Fabric Interrupt Status

The status of the MSS to the fabric interrupt, MSS_INT_M2F, can be monitored by reading the bit-band register bit of INTERRUPT_REASON0 and INTERRUPT_REASON1, as follows:

INTERRUPT_CTRL_BITBAND-> bit-band register bit of INTERRUPT_REASON0 or INTERRUPT_REASON1;

The following table gives the bit-band register bit of INTERRUPT_REASON0 and INTERRUPT_REASON1 in the INTERRUPT_CTRL structure. Refer to m2sxxx.h contained in the CMSIS folder.

Table 22-5. Bit-Band Register Bit of INTERRUPT_REASON0 and INTERRUPT_REASON1 (continued).
Bit-Band Register Bit
INTERRUPT_REASON0INTERRUPT_REASON1
SPIINT0_STATUSRESERVED5[3]
SPIINT1_STATUSMDDR_IO_CALIB_INT_STATUS
I2C_INT0_STATUSRESERVED6
I2C_INT1_STATUSFAB_PLL_LOCK_INT_STATUS
MMUART0_INTR_STATUSFAB_PLL_LOCKLOST_INT_STATUS
MMUART1_INTR_STATUSFIC64_INT_STATUS
MAC_INT_STATUSRESERVED7[24]
USB_MC_INT_STATUS
PDMAINTERRUPT_STATUS
HPD_XFR_CMP_INT_STATUS
TIMER1_INTR_STATUS
TIMER2_INTR_STATUS
CAN_INTR_STATUS
RTC_WAKEUP_INTR_STATUS
WDOGWAKEUPINT_STATUS
MSSDDR_PLL_LOCKLOST_INT_STATUS
ENVM_INT0_STATUS
ENVM_INT1_STATUS
I2C_SMBALERT0_STATUS
I2C_SMBSUS0_STATUS
I2C_SMBALERT1_STATUS
I2C_SMBSUS1_STATUS
HPD_XFR_ERR_INT_STATUS
MSSDDR_PLL_LOCK_INT_STATUS
SW_ERRORINTERRUPT_STATUS
DDRB_INTR_STATUS
ECCINTR_STATUS
CACHE_ERRINTR_STATUS
SOFTINTERRUPT_STATUS
COMBLK_INTR_STATUS
USB_DMA_INT_STATUS
RESERVED4

Example: The following code illustrates the usage of the MSS to the fabric interrupt in conjunction with the Timer1 interrupt.

int main()
{
    // STEP 1 - Enable Timer1 MSS to Fabric Interrupt (MSS_INT_M2F[10])
    INTERRUPT_CTRL_BITBAND->TIMER1_INTR_ENBL = 1;
    // STEP 2 - Configure Timer1 in PERIODIC MODE
    MSS_TIM1_init(MSS_TIMER_PERIODIC_MODE );
    // STEP 3 - Load count value
    MSS_TIM1_load_immediate(10000000 );
    // STEP 4 - Start Timer1
    MSS_TIM1_start();
    // STEP 5 - Enable Timer1 Interrupt and IRQ in NVIC
    MSS_TIM1_enable_irq();
    // Foreground loop
    for(;;)
    {
    	;
    }
    return 0;
}
/*
 * Connect MSS_INT_M2F[10] signal to LED.
 * Toggle LED on TIM1 interrupt.
 */
__attribute__((__interrupt__)) void Timer1_IRQHandler( void )
{
    uint32_t timer1_interrupt;
    // Read Timer1 MSS to Fabric Interrupt status
    timer1_interrupt = INTERRUPT_CTRL_BITBAND->TIMER1_INTR_STATUS;
    // Delay for extending the Timer1 MSS to fabric Interrupt pulse width
    delay(10000);
    /* Clear TIM1 interrupt */
    MSS_TIM1_clear_irq();
}