22.20.1 timer_add_clock_exception
Adds an exception to or from a pin with respect to a specified clock.
timer_add_clock_exception clock clock_name -pin pin_name -dir value
Arguments
-clock clock_nameSpecifies the name of the clock.
-pin pin_name
Specifies the exception on the pin in a synchronous network to be excluded from the specified clock period.
-dir value
Specifies direction.
| Value | Description |
|---|---|
| from | Refers to paths starting at the specific pin. |
| to | Refers to paths ending at the specific pin. |
Supported Families
All
Exceptions
For the ProASIC3/E, ProASICPLUS, ProASIC, Axcelerator, eX, and SX-A families, the timing analysis tool translates this command to an equivalent SDC command set_multicycle_path.
Examples
The following example adds a clock exception from the pin reg_q_a_10_/U0:CLK with respect to the clock clk.
timer_add_clock_exception clock {clk} -pin {reg_q_a_10_/U0:CLK} -dir {from}The
following example adds a clock exception to the pin reg_q_a_10_/U0:E with respect to the
clock clk.
timer_add_clock_exception clock {clk} -pin {reg_q_a_10_/U0:E} -dir {to}See
Alsotimer_remove_clock_exception
set_multicycle_pathTcl documentation conventions