22.20.17 timer_setenv_clock_period
timer_setenv_clock_period -clock clock_name \
[-unit {value} -period period_value \
[-dutycycle dutycycle]Arguments
-clock clock_name
Specifies the name of the clock for which to set the period.
-unit {value}
Specifies the unit for the clock period constraint. The default is ns. The following table shows the acceptable values for this argument:
| Value | Description |
|---|---|
| ns | nanoseconds |
| ps | picoseconds |
-period period_value
Specifies the period in the specified unit.
-dutycycle dutycycle
Specifies the duty cycle for the clock constraint.
Supported Families
All
Exceptions
For the ProASIC3/E, ProASICPLUS, ProASIC, Axcelerator, SXS, SX-A, and eX families, Microchip recommends that you use the equivalent SDC command create_clock.
Examples
The following example sets a clock period of 2.40ns on the clock clk1:
timer_setenv_clock_period -clock clkl unit (ns) -period 2.40
See Also
timer_setenv_clock_freq
Tcl documentation conventions