22.20.16 timer_setenv_clock_freq
Sets a required clock frequency for the specified clock in megahertz (MHz).
timer_setenv_clock_freq -clock clock name -freq value [-dutycycle dutycycle]Arguments
-clock clock_name
Specifies the name of the clock for which to set the required frequency.
-freq value
Specifies the frequency in MHz.
-dutycycle dutycycle
Specifies the duty cycle for the clock constraint.
Supported Families
All
Exceptions
For the ProASIC3/E, ProASICPLUS, ProASIC, Axcelerator, SXS, SX-A, and eX families, Microchip recommends that you use the equivalent SDC command create_clock.
Examples
The following example sets a clock frequency of 100MHz on the clock clk 1:
timer_setenv_clock_freq -clock {clkl} -freq 100.00
See Also
create_clock (SDC clock constraint)
Tcl documentation conventions
timer_setenv_clock_period