9.22.14.1 Setting Log window preferences

From the Preferences dialog box, you can change the text color of the messages that appear in the Log window.

To set Log window preferences:

  1. From the File menu, choose Preferences.
  2. Follow the directions in the Color Settings area or click the Restore Defaults button.
    Figure 9-162. Preferences
    ???
  3. Click OK to apply settings.
Note: You can clear the Log window by choosing Clear Log window from the Edit menu or you can automatically erase the information by checking the Clear Log Window Automatically checkbox.