2.1.13 ASB Advanced Options - SMEV Status
This option exposes status signals from the sample monitor and evaluation block (SMEV). These signals are useful for monitoring the current processing state of the SMEV.
The exposed SMEV status ports are listed in the following table.
| Port Name | Direction | Description |
|---|---|---|
| EV_DONE | Output | SMEV done. Indicates that the SMEV has completed processing for the current channel. |
| EV_EVFLAG | Output | SMEV active. Indicates that the SMEV is currently active for the channel that has just been sampled by the analog sample sequence controller (ASSC). |
| EV_CHHOLD[4:0] | Output | Channel value. Indicates the channel that the SMEV is currently processing. |