Description
This tcl command sets the temperature in the operating conditions to one of the predefined types.
smartpower_set_temperature_opcond -use {value}
Arguments
| Parameter | Type | Description | 
|---|
| use | string | Specifies the temperature in the operating conditions. The acceptable values for this argument are the following: - oprange - Sets the temperature in the operating conditions as specified in your Project Settings.
 - design - Sets the temperature in the operating conditions as specified in the SmartPower design-wide operating range. Applies to SmartPower only.
 - mode - Sets the temperature in the operating conditions as specified in the SmartPower mode-specific operating range. Applies to SmartPower only.
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'use' has illegal value. | 
| None | Required parameter 'use' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_set_temperature_opcond -use "oprange | design | mode"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
This example sets the temperature in the operating conditions as specified in the custom mode-settings:
smartpower_set_temperature_opcond -use {mode}