Description
This Tcl command sets the mode for cycle-accurate power analysis.
smartpower_set_mode_for_analysis -mode {value}
Arguments
| Parameter | Type | Description | 
|---|
| mode | string | Specifies the mode for cycle-accurate power analysis. This parameter is mandatory. The acceptable values for this argument are the following: - Active - The operating mode is set to Active.
 - Static - The operating mode is set to Static.
 - Flash*Freeze - The operating mode is set to
                                        Flash*Freeze(RTG4™, SmartFusion® 2, IGLOO® 2).
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'mode' is missing. | 
| None | Parameter 'mode' has illegal value. | 
| None | mode: Invalid argument value: 'mode_name' (expecting Active, Static or Flash*Freeze). | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_set_mode_for_analysis -mode "Active | Static | Flash*Freeze"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
The following example sets the mode for analysis to active:
smartpower_set_mode_for_analysis -mode {active}