Description
This Tcl command removes all initialization annotations for the specified mode.
Note: This command is associated with the functionality of Initialize frequencies and probabilities dialog box.
smartpower_remove_all_annotations [-opmode {value}]
Arguments
| Parameter | Type | Description | 
|---|
| opmode | string | Removes all initialization annotations for the specified mode, where value must be Active or
                                Flash*Freeze (RTG4, SmartFusion 2 and IGLOO 2). | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'opmode' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_remove_all_annotations [-opmode "Active"]'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
The following example initializes all clocks with opmode "Acitve":
smartpower_remove_all_annotations -opmode {Active}