Description
This Tcl command removes an existing clock or set domain.
smartpower_remove_domain -domain_name {domain name} -domain_type "set | clock"
Arguments
| Parameter | Type | Description | 
|---|
| domain_type | string | Specifies the type of domain to remove. The acceptable values for this argument are: - clock - The domain is a clock domain.
 - set - The domain is a set domain.
 
  | 
| domain_name | string | Specifies the name of the domain to remove. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'domain_name' is missing. | 
| None | Parameter 'domain_name' has illegal value. | 
| None | domain_type: Invalid argument value: 'value' (expecting set or clock). | 
| None | Could not delete domain 'domain name'. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_remove_domain -domain_name "domain name" -domain_type "set | clock"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
This example removes the clock domain names "myclk":
smartpower_remove_domain -domain_type {clock} -domain_name {myclk}
This example removes the set domain names "myset":
smartpower_remove_domain -domain_type {set} -domain_name {myset}