Description
This Tcl command sets the frequency of a pin in megahertz (MHz). If you do not use this command, each pin will have default frequency based on its domain.
Note: The pin_name must be the name of a pin that already exists in the design and already belongs to a domain. When specifying the unit, a space must be between the frequency value and the unit. Execute the "smartpower_commit" Tcl command for preserving any changes in SmartPower.
smartpower_set_pin_frequency -pin_name {pin_name} -pin_freq {value}
Arguments
| Parameter | Type | Description | 
|---|
| pin_freq | string | Specifies the value of the frequency in Hz, KHz and MHz, which can be any positive decimal number. | 
| pin_name | string | Specifies the name of the pin for which the frequency will be set. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'pin_name' is missing. | 
| None | Parameter 'pin_name' is missing or has invalid value. | 
| None | Required parameter 'pin_freq' is missing. | 
| None | Failed to set "pin name" pin frequency to 2.60 Hz. | 
| None | pin_freq: Parameter format incorrect (expecting a positive decimal value, optionally followed by a unit (possible values are Hz, KHz or MHz)). | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_set_pin_frequency [-pin_name "name of pin"]+ -pin_freq "decimal value [ unit { Hz | KHz | MHz } ]"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
This example sets the frequency of the pin named "d_in" to 100 MHz:
smartpower_set_pin_frequency -pin_name {d_in} -pin_freq {100}