Description
This Tcl command sets the mode of computing junction temperature.
Note: To compute the junction temperature, set the smartpower_set_thermalmode, smartpower_set_tambientand smartpower_set_cooling commands. The junction temperature will be updated when an output command is executed, such as report(Power).
smartpower_set_thermalmode [-mode {value}]
Arguments
| Parameter | Type | Description | 
|---|
| mode | string | Specifies the mode in which the junction temperature is computed. The acceptable values for this argument are the following: - ambient - The junction temperature will be iteratively computed with total static power.
 - opcond - The junction temperature will be given as one of the operating condition range valuesspecified in the device selection.
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'mode' is missing. | 
| None | Parameter 'mode' has illegal value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_set_thermalmode -mode "opcond | ambient"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
The following example sets the computing of the junction temperature to ambient mode:
smartpower_set_thermalmode -mode {ambient}