Description
This tcl command sets the probability value of a pin driving an enable pin. For I/Os, if you do not use this command, the probability of the IOEnableSet is used. For memories, if you do not use this command, the probability of the MemoriesEnableSet is used.
smartpower_set_pin_probability -pin_name "name of pin" -pin_proba "decimal value"
Arguments
| Parameter | Type | Description | 
|---|
| pin_name | string | Specifies the name of a pin for which the probability will be set. This pin must be the direct driver of an enable pin. There may be multiple -pin_name arguments. This is mandatory. | 
| pin_proba | decimal value | Specifies the value of the pin probability as a percentage(%), which can be any positive decimal between 0 and 100 inclusive. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'pin_name' is missing.  | 
| None | Failed to set "value" pin frequency to 11.00. | 
| None | pin_proba: Invalid argument value: 'value' (expecting decimal value). | 
| None | Parameter 'pin_proba' must be less than or equal to 100.000. | 
| None | Parameter 'pin_proba' must be a positive decimal value. | 
| None | ERROR in setSystemDomainIdOfPin. The pin indoes not exist. | 
| None | 'smartpower_set_pin_probability [-pin_name "name of pin"]+ -pin_proba "decimal value"'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
The following example sets the probability of the pin driving the enable pin of a bidirectional I/O:
smartpower_set_pin_probability -pin_name {mybibuf/U0/U1:EOUT} -pin_proba {50.4}
The following example sets the probability of the "in" and "out" pins:
smartpower_set_pin_probability -pin_name {in out} -pin_proba {50.4}