Description
Enter description here
smartpower_get_temperature [-what "TRUE | FALSE"] [-opcond "Best | Typical | Worst"]
Arguments
| Parameter | Type | Description | 
|---|
| what | boolean |  | 
| opcond | string | Specifies the operating condition. The acceptable values for this argument are the following: - Worst - The operating condition is set to worst case.
 - Typical - The operating condition is set to typical case.
 - Best - The operating condition is set to best case.
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'param_name' is not defined. | 
| None | what: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, false, ambient or opcond). | 
| None | opcond: Invalid argument value: 'value' (expecting Best, Typical or Worst). | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| RTG4™ | 
| IGLOO® 2 | 
Example
Enter example description here
smartpower_get_temperature  -what "TRUE" -opcond "Best"