Description
            
            This Tcl command creates a new custom scenario entering the scenario name, duration
                (total duration for the sequence must equal to 100%), and selecting previously
                defined operating modes for this sequence.
            smartpower_add_new_scenario -name {New Scenario name} \
                            [-description {description of scenario}] \
                            -mode {Mode_name:duration}
        Arguments
            
            | Parameter | Type | Description | 
|---|
| name | string | Specifies the name of the new scenario. | 
| description | string | Specifies the description of the new scenario. This parameter is
                                optional. | 
| mode | string | Specifies the previously defined mode(s) and duration(s) for the
                                specified scenario. This parameter is mandatory. There may be
                                multiple -mode arguments (see example below). | 
 
            | Return Type | Description | 
|---|
| None | None | 
 
        Error Codes
            
            | Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | Required parameter 'mode' is missing. | 
| None | mode: Invalid argument value: 'mode_name' (expecting Active,
                                Static or Flash*Freeze). | 
| None | The sum of the duration must be 100%. Current sum:
                                duration_value. | 
| None | Parameter 'param_name' is not defined. Valid command formatting
                                is 'smartpower_add_new_scenario -name "scenario name" [-description
                                "description"] [-mode "":""]+' | 
 
        Supported Families
            
            | Supported Families | Supported Versions | 
|---|
| PolarFire® | v12.4+ | 
| SmartFusion® 2 | v12.4+ | 
| RTG4™ | v12.4+ | 
| IGLOO® 2 | v12.4+ | 
| PolarFire SoC | v12.6+ | 
 
        Example
            
            This example creates a new scenario called "MyScenario" with the specified modes and
                durations:
            smartpower_add_new_scenario -name "MyScenario" -mode "Custom_1:50.00" \ 
             		    -mode "Custom_2:25.00" -mode "Active:25.00"