3.2.14 MLME_AssociateResp_t Struct
C
typedef struct mlme_associate_resp_tag {
/** This identifies the message as \ref MLME_ASSOCIATE_RESPONSE */
enum msg_code cmdcode;
/** The address of the device requesting association. */
uint64_t DeviceAddress;
/** The short device address allocated by the coordinator on successful
* association. This parameter is set to 0xffff if the association was
* unsuccessful. */
uint16_t AssocShortAddress;
/** The status of the association attempt. */
uint8_t status;
} MLME_AssociateResp_t;
Summary
MLME_AssociateResp_t holds the MLME-ASSOCIATE.response message structure.
Description
None
Remarks
None