3.2.25 MLME_GetConf_t Struct
C
typedef struct mlme_get_conf_tag {
/** This identifies the message as \ref MLME_GET_CONFIRM */
enum msg_code cmdcode;
/** The result of the request for PHY PIB attribute information.*/
uint8_t status;
/** The identifier of the MAC PIB attribute to get. */
uint8_t PIBAttribute;
#if ((defined MAC_SECURITY_ZIP) || (defined MAC_SECURITY_2006))
/** The index within the table of the specified MAC PIB attribute to set. */
uint8_t PIBAttributeIndex;
#endif
/** The value of the indicated MAC PIB attribute that was read. */
PibValue_t PIBAttributeValue;
} MLME_GetConf_t;
Summary
MLME_GetConf_t holds the MLME-GET.confirm message structure
Description
None
Remarks
None