3.2.9 MCPS_DataConf_t Struct
C
typedef struct mcps_data_conf_tag {
/** This identifies the message as \ref MCPS_DATA_CONFIRM */
enum msg_code cmdcode;
/** The handle associated with the MSDU being confirmed. */
uint8_t msduHandle;
/** The status of the last MSDU transmission. */
uint8_t status;
#ifdef ENABLE_TSTAMP
/** Optional. The time, in symbols, at which the data were transmitted. The
* value of this parameter will be considered valid only if the value of the
* status parameter is MAC_SUCCESS, if the status parameter is not equal to
* MAC_SUCCESS, the value of the Timestamp parameter shall not be used for
* any other purpose. The symbol boundary is described by macSyncSymbolOffset
* This is a 24-bit value, and the precision of this value shall be minimum
* of 20 bits, with the lowest 4 bits being the least significant. */
uint32_t Timestamp;
#endif
} MCPS_DataConf_t;
Summary
MCPS_DataConf_t holds the MCPS-DATA.confirm message structure
Description
None
Remarks
None