3.2.15 MLME_AssociateConf_t Struct
C
typedef struct mlme_associate_conf_tag {
/** This identifies the message as \ref MLME_ASSOCIATE_CONFIRM */
enum msg_code cmdcode;
/** The short device address allocated by the coordinator on successful
* association. This parameter will be equal to 0 x ffff if the association
* attempt was unsuccessful. */
uint16_t AssocShortAddress;
/** The status of the association attempt. */
uint8_t status;
} MLME_AssociateConf_t;
Summary
MLME_AssociateConf_t holds the MLME-ASSOCIATE.confirm message structure
Description
None
Remarks
None