3.2.35 MLME_PollReq_t Struct
C
typedef struct mlme_poll_req_tag {
/* This identifies the message as \ref MLME_POLL_REQUEST */
enum msg_code cmdcode;
/** The addressing mode of the coordinator to which the poll is intended.
* This parameter can take one of the following values: 2 = 16 bit short
* address, 3 = 64 bit extended address. */
uint8_t CoordAddrMode;
/** The PAN identifier of the coordinator to which the poll is intended. */
uint16_t CoordPANId;
/** The address of the coordinator to which the poll is intended. */
uint64_t CoordAddress;
} MLME_PollReq_t;
Summary
MLME_PollReq_t holds the MLME-POLL.request message structure
Description
None
Remarks
None