3.2.18 MLME_DisassociateConf_t Struct
C
typedef struct mlme_disassociate_conf_tag {
/** This identifies the message as \ref MLME_DISASSOCIATE_CONFIRM */
enum msg_code cmdcode;
/** The status of the disassociation attempt. */
uint8_t status;
/** The addressing mode of the device that has either requested
* disassociation or been instructed to disassociate by its coordinator. */
uint8_t DeviceAddrMode;
/** The PAN identifier of the device that has either requested disassociation
* or been instructed to disassociate by its coordinator. */
uint16_t DevicePANId;
/** The address of the device that has either requested disassociation or
* been instructed to disassociate by its coordinator. */
uint64_t DeviceAddress;
} MLME_DisassociateConf_t;
Summary
MLME_DisassociateConf_t holds the MLME-DISASSOCIATE.confirm message structure
Description
None
Remarks
None