3.2.6 WPAN_Pandescriptor_t Struct
C
typedef struct wpan_pandescriptor_tag {
/** Coordinator address specification in received beacon frame */
WPAN_AddrSpec_t CoordAddrSpec;
/** The current logical channel used by the network */
uint8_t LogicalChannel;
/** The current channel page occupied by the network */
uint8_t ChannelPage;
/** Superframe specification in received beacon frame */
uint16_t SuperframeSpec;
/** Set to true if the beacon is from a PAN coordinator accepting GTS requests */
bool GTSPermit;
/** LQI at which the beacon was received.Lower values represent poorer link quality. */
uint8_t LinkQuality;
#ifdef ENABLE_TSTAMP
/** Time at which the beacon frame was received, in symbol counts. This
* quantity shall be interpreted as only 24-bits, with the most significant
* 8-bits entirely ignored. */
uint32_t TimeStamp;
#endif
} WPAN_Pandescriptor_t;
Summary
This structure contain PAN descriptor information
Description
None
Remarks
None